iMX93 linux prebuilt image and flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX93 linux prebuilt image and flashing

跳至解决方案
4,484 次查看
KHL
Contributor I

Hi,

I dowloaded iMX93 evk prebuilt images "LF_v6.1.1_1.0.0_images_IMX93EVK", there are lots of dtb, bin files in the package. I wish to flash back the default images, which image should I flash and how ?

I tried using uuu to flash "imx-image-full-imx93evk.tar.zst", but an error pops up as per below 

KHL_1-1685623336248.png

I tried switch to using a linux host machine, the uuu outcome remains. What went wrong ?

Thanks.

 

0 项奖励
回复
1 解答
4,469 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

I suggest you use the next command with the board on USB serial download mode.

uuu -b emmc_all imx-image-full-imx93evk.wic

Best regards.

Jorge.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,470 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I hope you are doing well.

I suggest you use the next command with the board on USB serial download mode.

uuu -b emmc_all imx-image-full-imx93evk.wic

Best regards.

Jorge.

0 项奖励
回复
4,456 次查看
KHL
Contributor I

Thank you. It works.

0 项奖励
回复