iMX8QXP PMIC I2C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,177件の閲覧回数
MJames
Contributor I

Hi,

I have a custom board using iMX8QXP. It has an EEPROM and an RTC connected to the PMIC_I2C lines.

While looking into the reference manual (IMX8DQXPRM), I found the PMIC_I2C module at section 9.1.11- SCU Pin Assignments. Does this mean that the PMIC_I2C can be accessed only from the SCFW? Can the A35 core access the above I2C?

Could someone please clarify this?

Thanks in advance,

MJames

0 件の賞賛
返信
1 解決策
1,155件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are correct the PMIC is managed by the SCFW on a private I2C bus.

Best regards/Saludos,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,156件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are correct the PMIC is managed by the SCFW on a private I2C bus.

Best regards/Saludos,
Aldo.

0 件の賞賛
返信