iMX8QXP PMIC I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QXP PMIC I2C

Jump to solution
1,202 Views
MJames
Contributor I

Hi,

I have a custom board using iMX8QXP. It has an EEPROM and an RTC connected to the PMIC_I2C lines.

While looking into the reference manual (IMX8DQXPRM), I found the PMIC_I2C module at section 9.1.11- SCU Pin Assignments. Does this mean that the PMIC_I2C can be accessed only from the SCFW? Can the A35 core access the above I2C?

Could someone please clarify this?

Thanks in advance,

MJames

0 Kudos
Reply
1 Solution
1,180 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are correct the PMIC is managed by the SCFW on a private I2C bus.

Best regards/Saludos,
Aldo.

View solution in original post

0 Kudos
Reply
1 Reply
1,181 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are correct the PMIC is managed by the SCFW on a private I2C bus.

Best regards/Saludos,
Aldo.

0 Kudos
Reply