iMX8QM SCU/M4 RGPIO Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8QM SCU/M4 RGPIO Interrupt

跳至解决方案
2,979 次查看
sbertrand
Contributor III

Hi,

The iMX8QM has two M4 with their down peripherals. One of which is RGPIO or Rapid GPIO ( perhaps even Fast GPIO, FGPIO).

Does the M4 GPIO block has interrupt support ?

It would appear not to be the case since the SDK for the M4 cores do not have interrupt register. 
/** GPIO - Register Layout Typedef */
typedef struct {
  __IO uint32_t PDOR;                              /**< Port Data Output Register, offset: 0x0 */
  __O  uint32_t PSOR;                              /**< Port Set Output Register, offset: 0x4 */
  __O  uint32_t PCOR;                              /**< Port Clear Output Register, offset: 0x8 */
  __O  uint32_t PTOR;                              /**< Port Toggle Output Register, offset: 0xC */
  __I  uint32_t PDIR;                              /**< Port Data Input Register, offset: 0x10 */
  __IO uint32_t PDDR;                              /**< Port Data Direction Register, offset: 0x14 */
} GPIO_Type;
/** RGPIO - Register Layout Typedef */
typedef struct {
  __IO uint32_t PDOR;                              /**< Port Data Output Register, offset: 0x0 */
  __O  uint32_t PSOR;                              /**< Port Set Output Register, offset: 0x4 */
  __O  uint32_t PCOR;                              /**< Port Clear Output Register, offset: 0x8 */
  __O  uint32_t PTOR;                              /**< Port Toggle Output Register, offset: 0xC */
  __I  uint32_t PDIR;                              /**< Port Data Input Register, offset: 0x10 */
  __IO uint32_t PDDR;                              /**< Port Data Direction Register, offset: 0x14 */
} RGPIO_Type;
 
Furthermore, the SDK for the M4 cores does not list any RGPIO interrupt vector : 
M4_0_TPM_IRQn                = 19,               /**< Timer PWM Module */
  Reserved36_IRQn              = 20,               /**< Reserved */
  Reserved37_IRQn              = 21,               /**< Reserved */
  M4_0_LPIT_IRQn               = 22,               /**< Low-Power Periodic Interrupt Timer */
  Reserved39_IRQn              = 23,               /**< Reserved */
  Reserved40_IRQn              = 24,               /**< Reserved */
  M4_0_LPUART_IRQn             = 25,               /**< Low Power UART */
  Reserved42_IRQn              = 26,               /**< Reserved */
  M4_0_LPI2C_IRQn              = 27,               /**< Low-Power I2C - Logical OR of master and slave interrupts */
  Reserved44_IRQn              = 28,               /**< Reserved */
Is this correct ?
Is there any way to have GPIO interrupt in M4 firmware ? What are the constraints ?
Regards,
Stan
标记 (5)
0 项奖励
回复
1 解答
2,808 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Stan

RGPIO module has not interrupt capability, opposed to GPIO module

in LSIO subsystem.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,809 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Stan

RGPIO module has not interrupt capability, opposed to GPIO module

in LSIO subsystem.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------