iMX8QM SCU/M4 RGPIO Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM SCU/M4 RGPIO Interrupt

ソリューションへジャンプ
2,973件の閲覧回数
sbertrand
Contributor III

Hi,

The iMX8QM has two M4 with their down peripherals. One of which is RGPIO or Rapid GPIO ( perhaps even Fast GPIO, FGPIO).

Does the M4 GPIO block has interrupt support ?

It would appear not to be the case since the SDK for the M4 cores do not have interrupt register. 
/** GPIO - Register Layout Typedef */
typedef struct {
  __IO uint32_t PDOR;                              /**< Port Data Output Register, offset: 0x0 */
  __O  uint32_t PSOR;                              /**< Port Set Output Register, offset: 0x4 */
  __O  uint32_t PCOR;                              /**< Port Clear Output Register, offset: 0x8 */
  __O  uint32_t PTOR;                              /**< Port Toggle Output Register, offset: 0xC */
  __I  uint32_t PDIR;                              /**< Port Data Input Register, offset: 0x10 */
  __IO uint32_t PDDR;                              /**< Port Data Direction Register, offset: 0x14 */
} GPIO_Type;
/** RGPIO - Register Layout Typedef */
typedef struct {
  __IO uint32_t PDOR;                              /**< Port Data Output Register, offset: 0x0 */
  __O  uint32_t PSOR;                              /**< Port Set Output Register, offset: 0x4 */
  __O  uint32_t PCOR;                              /**< Port Clear Output Register, offset: 0x8 */
  __O  uint32_t PTOR;                              /**< Port Toggle Output Register, offset: 0xC */
  __I  uint32_t PDIR;                              /**< Port Data Input Register, offset: 0x10 */
  __IO uint32_t PDDR;                              /**< Port Data Direction Register, offset: 0x14 */
} RGPIO_Type;
 
Furthermore, the SDK for the M4 cores does not list any RGPIO interrupt vector : 
M4_0_TPM_IRQn                = 19,               /**< Timer PWM Module */
  Reserved36_IRQn              = 20,               /**< Reserved */
  Reserved37_IRQn              = 21,               /**< Reserved */
  M4_0_LPIT_IRQn               = 22,               /**< Low-Power Periodic Interrupt Timer */
  Reserved39_IRQn              = 23,               /**< Reserved */
  Reserved40_IRQn              = 24,               /**< Reserved */
  M4_0_LPUART_IRQn             = 25,               /**< Low Power UART */
  Reserved42_IRQn              = 26,               /**< Reserved */
  M4_0_LPI2C_IRQn              = 27,               /**< Low-Power I2C - Logical OR of master and slave interrupts */
  Reserved44_IRQn              = 28,               /**< Reserved */
Is this correct ?
Is there any way to have GPIO interrupt in M4 firmware ? What are the constraints ?
Regards,
Stan
ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,802件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stan

RGPIO module has not interrupt capability, opposed to GPIO module

in LSIO subsystem.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,803件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stan

RGPIO module has not interrupt capability, opposed to GPIO module

in LSIO subsystem.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------