iMX8QM QSPI Slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM QSPI Slave

1,209 Views
jars121
Contributor I

Hi,

I'm looking to interface an iMX8QM to an external MCU which provides a QSPI interface as the Master. I found this question from 2018 regarding QSPI slave on the iMX8QM, but have been unable to find anything in the documentation which states that the QSPI interface only supports Master mode. Is QSPI Slave mode possible with the iMX8QM controller? Any clarification would be greatly appreciated.

Thanks!

0 Kudos
Reply
1 Reply

1,197 Views
igorpadykov
NXP Employee
NXP Employee

Hi jars121

 

>QSPI Slave mode possible with the iMX8QM controller

 

sorry it is not supported, in particular FlexSPI has not special master/slave setting like ecspi

ECSPIx_CONREG(CHANNEL_MODE).

 

Best regards
igor

0 Kudos
Reply