Hi, all.
I would like to use the imx8qm-mek RS-232 connector (J37).
LPUART2( /dev/ttyLP2 ) is not enabled.
What should I do?
I made the following changes.
changes
・init.rc (/device/nxp/imx8q/mek_8q)
- Added the following code before "on boot".
chmod 0777 /dev/ttyLP2
・imx8qm-mek.dts (/vendor/nxp-opensource/kernel-imx/arch/arm64/boot/dts/freescale)
- changed the following code.
&lpuart2 {
pinctrl-0 = <&pinctrl_lpuart2>;
status = "okay";
};