iMX8QM LPDDR4 RPA Support ROW_Addresses == 17 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM LPDDR4 RPA Support ROW_Addresses == 17 ?

ソリューションへジャンプ
6,656件の閲覧回数
hexiaotao
Contributor II

   I have a problem with a customized iMX8QM  LPDDR4 ( 2 x 4GiB ) memory.

   The table below shows memory device configuration. 16Gb per channel,1 Rank per channel .

49B1E55D-8706-45ac-89B9-90813848CC99.png

2CB7C2BF-310A-459e-AA4D-6B866A73659D.png

      I configed MX8QM_B0_LPDDR4_RPA_1.6GHz_v20.xlsx file like this: Chip Selects used is 1 and Number of Row Addresses is 17.

BA468747-9676-4678-BB41-49FBF8E6D2E5.png

      But it doesn't pass when i use mx8_ddr_stress_test_ER14 DDR Tester tool. Config log seems like ok, but Stress Test Blocking at  [ t0.1: data is addr test ]. The log below is all Stress Test log.

============================================
        DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 2
Density per chip select:   4096MB
Density per controller is: 4096MB
Total density detected on the board is: 8192MB
Note: As this SoC has more than one DDR Controller, the calculated
      density assumes all controllers are being used. Adjust the tested
      density per your board configuration if not all controllers are used
Command Bus Training was executed
No DDR data training errors detected for DDRC0
No DDR data training errors detected for DDRC1
============================================
MX8QM: Cortex-A72 is found
*************************************************************************
DDR Stress Test Iteration 1
  --------------------------------
  --Running DDR test on region 1--
  --------------------------------
t0.1: data is addr test
....
t0.2: row hop read test
...
t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test
....................................................................
t4: IRAM_to_DDRv1 test
...
t5: IRAM_to_DDRv2 test
  --------------------------------
  --Running DDR test on region2--
  --------------------------------
t0.1: data is addr test
...
How can i do to fix this problem? or does iMX8QM platform support this LPDDR4 memory device?
Thanks.
ラベル(1)
0 件の賞賛
返信
1 解決策
6,566件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi [email protected]‌,

Thanks for your patience, now SCFW lilmits the DDR size to 6GB both in DDR tool and Linux BSP.

1. Replace mx8qmb0_scfw_download.bin in DDR_tool/bin with the attached binary. You can stress test all 8GB memory size with your DDR script.

2. Modify board_system_config() in board.c in your SCFW project as follows

/* Board has 6GB8GB memory so fragment upper region and retain 4GB */

        BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL, 0xA00000000ULL,

            0xFFFFFFFFFULL));

Hope this help you.

Regards,

Israel H.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
6,566件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi [email protected]‌,

Could you please tell us which version of the SCFW and kernel linux are you using? Just to know if the programing aid that you are using is compatible.

Regards,

Israel H.

0 件の賞賛
返信
6,566件の閲覧回数
hexiaotao
Contributor II

Hi israelhernandez

      SCFW : imx-scfw-porting-kit-1.5.0

      linux kernel version 5.4.24

      Android SDK is : imx-android-10.0.0_2.3.0

0 件の賞賛
返信
6,567件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi [email protected]‌,

Thanks for your patience, now SCFW lilmits the DDR size to 6GB both in DDR tool and Linux BSP.

1. Replace mx8qmb0_scfw_download.bin in DDR_tool/bin with the attached binary. You can stress test all 8GB memory size with your DDR script.

2. Modify board_system_config() in board.c in your SCFW project as follows

/* Board has 6GB8GB memory so fragment upper region and retain 4GB */

        BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL, 0xA00000000ULL,

            0xFFFFFFFFFULL));

Hope this help you.

Regards,

Israel H.

0 件の賞賛
返信
6,217件の閲覧回数
simonng
Contributor III

Hi Israel H.,
I am using the iMX8M. The LPDDR4 that I am using is 4GB with 1 CS. I want to test the LPDDR4 using the DDR Tool v3.1. I set the density to 32Gb and set the Row to 17. But the DDR Tool still show the Row size is 16. The RPA is v24. Can you provide the firmware that can support the 17 bit row?

Here is the DDR Tool log:

*************************************************************************
MX8 DDR Stress Test V3.10
Built on Feb 5 2020 14:08:44
*************************************************************************

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x91d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 800MHz
DDR Clock: 1600MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 2048MB
Total density detected on the board is: 2048MB
============================================

MX8M: Cortex-A53 is found

*************************************************************************

 

Regards,

Simon

0 件の賞賛
返信
6,199件の閲覧回数
simonng
Contributor III

Hi,

Anyone can help on this issue? I do need this support in order to use LPDDR4 devices with 17 row.

Thanks,

Simon

0 件の賞賛
返信