iMX8QM Android Automotive Bootloader Image Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8QM Android Automotive Bootloader Image Issue

跳至解决方案
2,051 次查看
cbl
Contributor V

Hello,

I built Android Automotive 12.0.0_2.1.0(Linux 5.15.32 BSP) for the iMX8QM platform.

I tried to write the Bootloader image to the SD card with the command "sudo dd if=flash.bin of=/dev/sdb bs=1K seek=1".

When I insert the SD card into the board, I can't see any boot activity in the Debug console.

Then I wrote the "bootloader-imx8qm.img" and "u-boot-imx8qm-mek-uuu.imx" files to the SD card using the same dd command, but I could not see a boot movement in the Debug console.

What bootloader binary do I need to use to see a U-Boot stream in the Debug console?

Also, could you suggest a dd command to write the bootloader image to the SD card?

What should the "seek", "bs" and "count" parameters be for the iMX8QM in the dd command I will use?

Could you please help with these issues?

Best regards,

Efecan

 

0 项奖励
回复
1 解答
2,041 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

You need to erase everything to burn again your sd, The first commends to burn is uboot with bootloader-imx8qm.img" with bs=1K seek=1 but You have to use DDD to burn everything in android.

 

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,042 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

You need to erase everything to burn again your sd, The first commends to burn is uboot with bootloader-imx8qm.img" with bs=1K seek=1 but You have to use DDD to burn everything in android.

 

Regards

0 项奖励
回复