iMX8MQ processor Socket Based EVK for secure boot (OTP)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8MQ processor Socket Based EVK for secure boot (OTP)

2,007 次查看
nilesh_patel
Contributor II

Hi,

We are planning to work for a secure Boot on iMX8MQ.

For secure boot, we need to program the fuses on i.MX8MQ(processor) and as per our understanding this is a one-time programmable process.

So in the development phase, we would require process steps where
1) A method by which we can reverse the false written fuses? As per our understanding this is not possible. Kindly confirm.
2) An EVK which contains the socket-based processor, whose processor chipset can be replaced. Request to provide the reference where such EVK with processor socket for our development.

Thanks,

Nilesh Patel

标记 (3)
0 项奖励
回复
3 回复数

1,912 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nilesh

1. yes this understanding is correct.

2. EVK board design files have bom file which lists all used parts.

i.MX 8M Evaluation Kit | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,912 次查看
nilesh_patel
Contributor II

Hi igor,

Is there any method, to avoid processor damage?

Thanks,

Nilesh Patel

0 项奖励
回复

1,912 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nilesh

 

>Is there any method, to avoid processor damage?

I am afraid no, as blown fuses can not be reverted back.

 

Best regards
igor

0 项奖励
回复