iMX8MP MIPI DSI Commands Timing Out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP MIPI DSI Commands Timing Out

Jump to solution
11,266 Views
liamsul42
Contributor II

Hello,

I am running into an issue when trying to send MIPI DSI initialization commands from a iMX8MP to a ST7701S Panel Driver on a ER-TFT040-2 LCD Panel.  After attaching to the bridge, I am attempting to send the initialization commands, but get the error "mipi_dsi: wait payload tx done time out" on every single one of the commands. This is also causing the board to not boot as the Kernel panics with the error "Kernel panic - not syncing: Asynchronous SError Interrupt." I have included my ST7701S panel driver and kernel log as apart of this, any solutions or help would be greatly appreciated!

0 Kudos
Reply
1 Solution
11,175 Views
liamsul42
Contributor II

Thank you for the feedback, however, this was not the issue.

I ended up finding what the issue was and in the ST7701 driver the initialization function was being called by the prepare function which was happening prior to the clock starting. Hence, the error because none of the tx bits were being removed from queue with the clock not active. Moving the initialization function to happen before the enable and after the clock was activated fixed it.

View solution in original post

0 Kudos
Reply
7 Replies
11,125 Views
liqing1
Contributor I

hello liamsul42,I have the same situation, I tried several methods and it didn't work. could you tell me exactly how to move, thank you very much!

0 Kudos
Reply
11,012 Views
liamsul42
Contributor II

I was only getting this error due to the clock not running and not being able to clock out any bits from the FIFO queue that was sending the MIPI DSI commands. I would recommend ensuring that your clock is running and able to send out the packets/payloads from the FIFO queue.

0 Kudos
Reply
10,988 Views
liqing1
Contributor I

Thanks for your advice.I can get LPDT data with a logic analyzer, so the timeout is not important for me, I commented this code.

0 Kudos
Reply
11,190 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

such exceptions can be due to memory errors, one can run ddr test and

rebuild image.

https://community.nxp.com/docs/DOC-340179 

Also please check that you did not copied some binaries from previous builds

or other kernel revisions. Recommended fully rebuild image with modified sources.

Regards

0 Kudos
Reply
11,176 Views
liamsul42
Contributor II

Thank you for the feedback, however, this was not the issue.

I ended up finding what the issue was and in the ST7701 driver the initialization function was being called by the prepare function which was happening prior to the clock starting. Hence, the error because none of the tx bits were being removed from queue with the clock not active. Moving the initialization function to happen before the enable and after the clock was activated fixed it.

0 Kudos
Reply
9,988 Views
H_Grobben
Contributor I

This did the trick for me, partially. Do get an image, but my vertical line count seems off, image is replicated 2.5 times vertically.

I also removed the IOVCC and VCC in the device tree..

0 Kudos
Reply
10,791 Views
Udhay_
Contributor III

@liamsul42 

Hi,

if i move st7701_init_sequence(st7701) this function to st7701_enable but it is streaming and not able to see the data

Can you please share the code to u[email protected]

 

0 Kudos
Reply