iMX8MM keyctl add trusted, add_key: No such device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8MM keyctl add trusted, add_key: No such device

跳至解决方案
400 次查看
mariusoctavian
Contributor IV

Hi,
This is iMX8MM built with yocto scarthgap.

I am following mainly this doc-stm in conjunction with this doc


all optee-os optee-test and optee are in the build.

The Kernel config looks like:

CONFIG_CRYPTO_HASH=y
CONFIG_CRYPTO_AES=y
CONFIG_MD=y 
CONFIG_DM_CRYPT=y
CONFIG_BLK_DEV_DM=y
CONFIG_KEYS=y
CONFIG_TRUSTED_KEYS=m
CONFIG_ENCRYPTED_KEYS=y
CONFIG_TRUSTED_KEYS_TEE=y

 

The drivers looks okay

[root@imx:~$ dmesg | grep optee
[    1.530781] optee: probing for conduit method.
[    1.530800] optee: revision 4.2 (c6be5b57)
[    1.532316] optee: dynamic shared memory is enabled
[    1.559229] optee: initialized driver

 

The xtest passes

+-----------------------------------------------------
43430 subtests of which 0 failed
155 test cases of which 0 failed
0 test cases were skipped
TEE test application done!

 

But

[root@imx:~$ keyctl add trusted kmk "new 32" @s
add_key: No such device
[root@Dekoda:~$ 

 

 fails with,

No such device,

dmesg shows nothing

 

0 项奖励
回复
1 解答
370 次查看
mariusoctavian
Contributor IV

I do this, we have all HAB TC enabled.
I found the problem.
I was using the 5.15.60 kernel due custom drivers.
As the results did not make any sense I  replaced for the time being with 6.6.23 and all good.

I can add trusted key to KR session and
use dm to encrypt a partition using the key blob.

RESOLVED

在原帖中查看解决方案

0 项奖励
回复
2 回复数
376 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello, 

On the MX8MM DEK blob must be created by a software running in Arm TrustZone Secure World, the CAAM block takes into consideration the TrustZone configuration when encapsulating the DEK and the resulting blob can be only decapsulated by a SW running in the same configuration. As ROM code is running in ARM TrustZone secure world we must encapsulate the blobs using OP-TEE.

Please check this thread:

https://community.nxp.com/t5/i-MX-Processors/Enabling-OP-TEE-in-i-MX8MM-EVK-FIT-image/m-p/1160604

 

Regards

0 项奖励
回复
371 次查看
mariusoctavian
Contributor IV

I do this, we have all HAB TC enabled.
I found the problem.
I was using the 5.15.60 kernel due custom drivers.
As the results did not make any sense I  replaced for the time being with 6.6.23 and all good.

I can add trusted key to KR session and
use dm to encrypt a partition using the key blob.

RESOLVED

0 项奖励
回复