iMX8MM EVK Linux boot fails with demo image out of the box

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MM EVK Linux boot fails with demo image out of the box

3,336 Views
davidvescovi
Contributor V

Brand new i.MX 8M Mini DDR4 EVK out of the box.

Android SD card boots fine.

Downloaded L5.4.47-2.2.0_images_MX8MMEVK.zip and extracted.

Burned imx-image-full-imx8mmevk.wic to SD card and booted.

...

[ 968.744636] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 1024
U-Boot SPL 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Sep 11 2020 - 22:00:22 +0000)
power_bd71837_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
Training FAILED

 

0 Kudos
Reply
8 Replies

3,309 Views
davidvescovi
Contributor V

got it working ... no help from printed documentation.

0 Kudos
Reply

3,161 Views
jrsalas
Contributor I

May I know if you found a 'ready' .wic image for the 8MMINID4-EVK (not 8MMINILPD4-EVK)? or did you have to go the hard way for an 'out-of-the-box' demo?
Thanks!

0 Kudos
Reply

3,135 Views
jrsalas
Contributor I

Hi, thanks for you reply.

The output I get is:

U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 03 2020 - 22:30:26 +0000)
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
Training FAILED

About the second line above 'Can't find PMIC:PCA9450'. Looking into schematics for 8MMINID4, U8 (PMIC) is ROHM BD71847MWV not PCA9450 as in 8MMINILPD4. Could this be the reason why I cannot boot the prebuilt wic image on my new EVB? Note that it works with preloaded Android SD.

Thanks again!

0 Kudos
Reply

3,129 Views
davidvescovi
Contributor V

My issue was the newer evk boards use the DDR4 memory as opposed to LPDDR4 used on the original evk boards.

The prebuilt demo image was built using LPDDR4 and does not run on DDR4 evks.  (unless NXP has updated it) in my case. Check your evk part numbers.

I had to rebuild image for DDR4 to get it to run on DDR4 based evk.

 

 

David

0 Kudos
Reply

3,147 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, just now I download wic of 5.4.70 to the imx8mmddr4 evk board successfully, you can use it

0 Kudos
Reply

3,319 Views
davidvescovi
Contributor V

maybe you should improve the documentation as the procedure as described in the quick start manual is wrong.

3,314 Views
joanxie
NXP TechSupport
NXP TechSupport

you can find the specific ddr4 in the dts or uboot image name, if you use ddr4 board, try to choose that

0 Kudos
Reply

3,323 Views
joanxie
NXP TechSupport
NXP TechSupport

my understanding is that this image is for imx8mm lpddr4 board, if  you use ddr4 board, try to use the specific uboot for ddr4 board and test again

0 Kudos
Reply