Hi all!
I'm trying to change the trip points of the iMX8MM device tree:
thermal-zones {
cpu-thermal {
polling-delay-passive = <250>;
polling-delay = <2000>;
thermal-sensors = <&tmu>;
trips {
cpu_alert0: trip0 {
temperature = <85000>;
hysteresis = <2000>;
type = "passive";
};
cpu_crit0: trip1 {
temperature = <95000>;
hysteresis = <2000>;
type = "critical";
};
};
cooling-maps {
map0 {
trip = <&cpu_alert0>;
cooling-device =
<&A53_0 THERMAL_NO_LIMIT THERMAL_NO_LIMIT>,
<&A53_1 THERMAL_NO_LIMIT THERMAL_NO_LIMIT>,
<&A53_2 THERMAL_NO_LIMIT THERMAL_NO_LIMIT>,
<&A53_3 THERMAL_NO_LIMIT THERMAL_NO_LIMIT>;
};
};
};
};
I'm trying to update the values from 85C to 95C and from 95C to 105C. However, when I compile the device tree and check the /sys/class/thermal/thermal_zone0/trip_point_0_temp, the values are the default ones: 85C and 95C.
Tested on NXP kernel 5.4 and 5.15. Does anyone know what's happening? Is this a bug or I should configure the device tree in a different way?
Tested on iMX8MM DL and iMX8MP.
Thanks!
Hi
You need change source code based on a yocto patch or using devtool modify linux-imx
Here is my test result based on devtool:
root@imx8mp-lpddr4-evk:~# cat /sys/class/thermal/thermal_zone0/trip_point_0_temp
95000
root@imx8mp-lpddr4-evk:~# cat /sys/class/thermal/thermal_zone0/trip_point_1_temp
105000
Hi @Zhiming_Liu, thanks for the reply.
As far as I understand, for iMX8M, the code that I should look at is imx8mm_thermal.c, the imx_thermal.c is not being used in this case. Am I correct?
Best Regards,
Hiago.
Hi @hfranco
Correct, let me test and give you answer about this issue.