iMX8M mini custom board fails in uuu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M mini custom board fails in uuu

ソリューションへジャンプ
3,804件の閲覧回数
raymondman
Contributor II

After passing the DDR RAM stress test, I copy the lpdd4_timing.c to u-boot source code tree and also modify imx8mm_evk.h with the following changes

#define PHYS_SDRAM_SIZE    0x40000000 //1GB

#define CONFIG_MXC_UART_BASE    UART1_BASE_ADDR//use UART1 as debug console

Then I generate a new imx-boot-imx8mmevk-sd.bin-flash_evk in Yocto.

The boot mode is set to the same as the reference design, i.e.

BOOT_CFG1,2,5,6,11 & 13 have 10Kohm pull high resistors. All other BOOT_CFG are left unconnected.

>uuu -v -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk

**************************************

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.191-0-g411f78f

Your console don't support VT mode, fail back to verbose mode
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152

Run built-in script:

uuu_version 1.2.39

# @_flash.bin | bootloader
# @_image [_flash.bin] | image burn to emmc, default is the same as bootloader

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl
SDPV: jump
# }

FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: Done


Wait for Known USB Device Appear...
New USB Device Attached at 1:1
1:1>Start Cmd:SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk
100%1:1>Okay (1.296s)
New USB Device Attached at 1:1
1:1>Start Cmd:SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk
100%1:1>Okay (1.301s)

**************************************

The image is downloaded to the SoC several times but cannot be programmed to the eMMC.

Can anyone give me any hints how to resolve it?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,776件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,
 
In your custom board do you have a type-C connector as in the EVK?

You may refer to the following community thread:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-US...

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,798件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the UART log when trying to flash uboot?

BR,
Aldo.

0 件の賞賛
返信
3,792件の閲覧回数
raymondman
Contributor II

Hi Aldo,

Please see the log below.

U-Boot SPL 2021.04-5.10.35-2.0.0+g3463140881 (Jun 08 2021 - 01:39:44 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from USB SDP
g_dnl_register: failed!, error: -19
SDP dnl register failed: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

Please advise.

0 件の賞賛
返信
3,786件の閲覧回数
raymondman
Contributor II

Hi Aldo,

Enable the debug messages in spl.c but it seems useless.

U-Boot SPL 2021.04-5.10.35-2.0.0+g3463140881 (Jan 20 2022 - 19:35:03 +0800)
spl_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
>>SPL: board_init_r()
SEC0: RNG instantiated
Normal Boot
Trying to boot from USB SDP
g_dnl_register: g_dnl_driver.name = usb_dnl_sdp
g_dnl_register: failed!, error: -19
SDP dnl register failed: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

error code 19 is no device.

I use the information of the article (https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Manually-build-Boot-binary-for-i-MX8M-Mi...  to create the flash.bin again but the same result.

As I use USB to download the flash.bin successfully, I do not understand why SPL cannot find the USB. Please help.

0 件の賞賛
返信
3,777件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,
 
In your custom board do you have a type-C connector as in the EVK?

You may refer to the following community thread:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-US...

Best regards,
Aldo.

0 件の賞賛
返信