iMX8M mini + PCA9450

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M mini + PCA9450

2,374件の閲覧回数
giacomobiancala
Contributor I

Hi,

I am developing custom board based on iMX8M mini + PCA9450.

Is it possible to use internal RTC with backup battery? I suppose there is no possibility on PCA9450.

Is it necessary to use external RTC I2C IC?

Thanks,

Giacomo

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,218件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo

I believe you are right, as PCA9450 has not separate LICELL input as for example

PF4210.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,218件の閲覧回数
giacomobiancala
Contributor I

Thank you Igor!

0 件の賞賛
返信