IMX287 Power on Fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX287 Power on Fail

2,613件の閲覧回数
nwpuxhy
Contributor I

     I designed a product  using iMX287 as MCU.Most of the time  the product work normal,sometimes the product does not work with boot fail . The probability is one in dozens.  In this abnormal condition ,the device will continuously ‘died’ until turn off the 5V power and turn on it.  I found the VDDIO drop down to 3.1V, VDDD drop down to 1.05V and VDDA drop down to 1.04V.I don't know why this happened, and I also don't know in which condition this will happen. How can I solve this problem?  Is there some problem with my schematic?  I use 5V only  source .

Best regards.I

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,527件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 许辉勇 许 

may be useful to look on

Brown out issues on ConnectCard (Wi)i.mx28 modules | Digi International 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,527件の閲覧回数
nwpuxhy
Contributor I

It.s not same with that.When the  iMX287 boot failed,the device will continuously ‘died’ until turn off the 5V power and turn on it.At the same time,the VDDIO drop down to 3.1V, VDDD drop down to 1.05V and VDDA drop down to 1.04V.

0 件の賞賛
返信