iMX8M mini + 2GB DDR4 boot problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M mini + 2GB DDR4 boot problems

1,729件の閲覧回数
giacomobiancala
Contributor I

Dear all,

I have some booting problems on my custom board based on iMX8M mini processor.

We use PMIC PCA9450.

Processor code MIMX8MM5DVTLZAA

DDR4 DRAM code (2GB total): 2 x MT40A512M16LY-075:E

DRAM Schematics connections is the same than EVK SCH-35104_B1  (8MMINID4-CPU).

We set main voltage as follows:

- VDD_DRAM&PU = 0,9V

- VDD_DRAM_1V2 = 1,2V

We produced 14 prototipes of this board. 10 boards always boot properly and they have no problems.

The other 4 boards do not boot properly every time. Console output is following:

U-Boot SPL 2018.03-g5f7f913-dirty (Jul 03 2020 - 13:57:13 +0200)
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED

There are 2 FAILED on DRAM test so the boot process stops.

If I run RAM Stress Test "mscale_ddr_tool_v310_setup.exe" (both calibration and Stress Test) all works fine so it seems that DDR4 connections have no problems but when I use the UBOOT the booting stops after RAM tests in SPL (only on this 4 boards).

Could you help me?

Thanks

Giacomo

ラベル(1)
0 件の賞賛
返信
1 返信

1,574件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo

if only some boards do not boot properly, this may be poor soldering issue,

one can try to test boards with x-ray screening.

Alternatively one can try to tweak drive strength and ODT parameters using

RPA tool on i.MX 8M Family DDR Tool Release 
Check power supply noise or spikes – refering to HW Developers Guide

i.MX 8M Mini Hardware Developer’s Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信