iMX8M is possible to use a Single SPI device on QSPI Interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M is possible to use a Single SPI device on QSPI Interface?

1,795 Views
leandroschmitz
Contributor I

I need add 3x CAN bus and 4x 12 bits Analog Interface to my iMX8M Computer On Module.

To do these I need a extra SPI bus, I'd like to know if is possible to use the QSPI Interface .

Thanks

Regards

Leandro Schmitz

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,555 Views
igorpadykov
NXP Employee
NXP Employee

Hi Leandro

yes possible and for example it is described in

Figure 10-17. Serial Flash Access Scheme i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply