iMX8M enable two QSPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8M enable two QSPI

2,615 次查看
charleshuang
Senior Contributor II

Hi,

I want to know how to enable two qspi

My setting as below

&qspi {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_qspi>;
        status = "okay";
        flash0: n25q256a@0 {
                reg = <0>;
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "micron,n25q256a";
                spi-max-frequency = <29000000>;
                spi-nor,ddr-quad-read-dummy = <6>;
        };
        flash1: n25q256a@1 {
                reg = <1>;
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "micron,n25q256a";
                spi-max-frequency = <29000000>;
                spi-nor,ddr-quad-read-dummy = <6>;
        };
};
                pinctrl_qspi: qspigrp {
                        fsl,pins = <
                                MX8MQ_IOMUXC_NAND_ALE_QSPI_A_SCLK       0x82
                                MX8MQ_IOMUXC_NAND_CE0_B_QSPI_A_SS0_B    0x82
                                MX8MQ_IOMUXC_NAND_DATA00_QSPI_A_DATA0   0x82
                                MX8MQ_IOMUXC_NAND_DATA01_QSPI_A_DATA1   0x82
                                MX8MQ_IOMUXC_NAND_DATA02_QSPI_A_DATA2   0x82
                                MX8MQ_IOMUXC_NAND_DATA03_QSPI_A_DATA3   0x82
                                MX8MQ_IOMUXC_NAND_CLE_QSPI_B_SCLK       0x82
                                MX8MQ_IOMUXC_NAND_CE2_B_QSPI_B_SS0_B    0x82
                                MX8MQ_IOMUXC_NAND_DATA04_QSPI_B_DATA0   0x82
                                MX8MQ_IOMUXC_NAND_DATA05_QSPI_B_DATA1   0x82
                                MX8MQ_IOMUXC_NAND_DATA06_QSPI_B_DATA2   0x82
                                MX8MQ_IOMUXC_NAND_DATA07_QSPI_B_DATA3   0x82
                        >;
                };

but it's not working, and it will hang system and kernel panic message
The attached is the dmesg

0 项奖励
回复
1 回复

2,432 次查看
igorpadykov
NXP Employee
NXP Employee

Hi charles

for two qspi one can look at below example:

linux/arch/arm64/boot/dts/freescale/fsl-imx8mq-ddr3l-arm2.dts

fsl-imx8mq-ddr3l-arm2.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

and description in sect.3.5 Quad Serial Peripheral Interface (QuadSPI) attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复