iMX8M SAI I8S support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M SAI I8S support

ソリューションへジャンプ
3,132件の閲覧回数
aelder
Contributor III

The datasheet description for the iMX8M states 

Five SAI (synchronous audio interface) modules supporting I2S, AC97, TDM, and
codec/DSP interfaces, including one SAI with 8 TX and 8 RX lanes, one SAI with 4
TX and 4 RX lanes, and three SAI with 1 TX and 1 RX lanes. Supports over 20
channels of audio

Am I correct in assuming the SAI with 8 TX and 8 RX lanes can be configured to support I8S (8 channel TDM on each lane, making for a total of 64 channels of audio in and 64 channels of audio out?

ラベル(2)
タグ(2)
1 解決策
2,891件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

>I correct in assuming the SAI with 8 TX and 8 RX lanes can be configured to support I8S

>(8 channel TDM on each lane, making for a total of 64 channels of audio in and 64 channels of audio out?

yes correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,892件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

>I correct in assuming the SAI with 8 TX and 8 RX lanes can be configured to support I8S

>(8 channel TDM on each lane, making for a total of 64 channels of audio in and 64 channels of audio out?

yes correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------