iMX8M Plus PCIe prefetchable memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M Plus PCIe prefetchable memory

ソリューションへジャンプ
2,248件の閲覧回数
kentmeyer
Contributor II

Per the post https://community.nxp.com/t5/i-MX-Processors/Can-not-allocate-PCIe-region-when-size-is-8M-on-Sabre-p... we see that the IMX6 PCIe driver cannot support prefetchable memory regions of more than 16MBytes in the 

Is this limitation still in place and applicable to the IMX8M Plus PCIe as well? 

Thanks.

0 件の賞賛
返信
1 解決策
2,242件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kentmeyer 
Hello,

  According to section 2.2 (Cortex-A53 Memory Map) of i.MX 8M Plus
Reference Manual (Rev. 1, 06/2021) the following memory address
area of 128MB is located for the PCIe: 1800_0000 - 1FFF_FFFF

  Under Linux:
— PCIe host configuration space: 0x33c0_0000 – 0x33ff_ffff (4Mbytes)
— PCIe device configuration space: 0x27f0_0000 – 0x27f7_ffff (512K bytes)
— PCIe IO space: 0x27f8_0000 – 0x27f8_ffff (64K bytes)
— PCIe memory space: 0x2000_0000 – 0x27ef_ffff (127M bytes)

 

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,243件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kentmeyer 
Hello,

  According to section 2.2 (Cortex-A53 Memory Map) of i.MX 8M Plus
Reference Manual (Rev. 1, 06/2021) the following memory address
area of 128MB is located for the PCIe: 1800_0000 - 1FFF_FFFF

  Under Linux:
— PCIe host configuration space: 0x33c0_0000 – 0x33ff_ffff (4Mbytes)
— PCIe device configuration space: 0x27f0_0000 – 0x27f7_ffff (512K bytes)
— PCIe IO space: 0x27f8_0000 – 0x27f8_ffff (64K bytes)
— PCIe memory space: 0x2000_0000 – 0x27ef_ffff (127M bytes)

 

Regards,
Yuri.

0 件の賞賛
返信