[iMX8M Plus][ISP] Flicker Advoidance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX8M Plus][ISP] Flicker Advoidance

ソリューションへジャンプ
1,878件の閲覧回数
khang_letruong
Senior Contributor III

Dear Community,

From the guidance for the VVEXT tool made by one of NXP's partners, it says :

Flicker Avoidance Period

The ISP offers the feature of flicker suppression. The flicker suppression aims at the suppression of brightness fluctuations of the image, which are caused by differences in the frequencies of the light source (e.g. fluorescent lamps, LEDs) and the image acquisition frequency (beatings).

This feature has not yet been put into operation by PHYTEC and is therefore not supported for the time being.

We are experiencing the same issue. Therefore, I would like to know if this feature would generically be NXP's ISP feature or specifically to PHYTEC's implementation, please ?

Thanks in advance and best regards,

Khang

0 件の賞賛
返信
1 解決策
1,850件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I have confirmed that ISP doesn't support this currently, if customer needs it,  need consult ISP vendor for more detailed information, maybe it's not free, if you need it, pls consult local DFAE to get further help

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,851件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I have confirmed that ISP doesn't support this currently, if customer needs it,  need consult ISP vendor for more detailed information, maybe it's not free, if you need it, pls consult local DFAE to get further help

0 件の賞賛
返信
1,862件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

let me double check it and tell you later

0 件の賞賛
返信