Hi,
I understand iMX8MPlus supports 2 x 4 lane MIPI CSI-2, i.e. it supports 2 camera each with 4 lane MIPI CSI-2. Can it support a single camera (single image sensor) that requires 2 x 4 lane MIPI CSI-2?
Hi Joan,
I understand each MIPI can support up to 4 lanes.
Can I combine both MIPI 4 lanes to handle a single image sensor that requires 2 x 4 lanes MIPI CSI interface? One example is OMNIVISION’s OV13870. Can iMX8M Plus support this OMNIVISION image sensor? Can the iMX8M Plus merge data from both the MIPI interface to become a single image? Or it will always treat both MIPI interface as 2 separate images?
Usually image sensors with higher number of pixels (> 10MPix) will require more than 4 lanes due to the speed limitation of each lane.
Can iMX8M Plus support this OMNIVISION image sensor?
>yes, current bsp supports ov2775 and ov5640 as default
Usually image sensors with higher number of pixels (> 10MPix) will require more than 4 lanes due to the speed limitation of each lane.
>imx8mp mipi csi can support 1.5Gx4=6Gbps, if your sensor is 10M@30, this is 10x30x16=4.8G<6G, and you can current ISP can support up to 12M camera, so I don't think you need use dual mipi csi to one camera