iMX8M Plus - 8 Lane CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Plus - 8 Lane CSI

3,717 Views
MPUUser
Contributor I

Hi,

I understand iMX8MPlus supports 2 x 4 lane MIPI CSI-2, i.e. it supports 2 camera each with 4 lane MIPI CSI-2. Can it support a single camera (single image sensor) that requires 2 x 4 lane MIPI CSI-2?

0 Kudos
Reply
6 Replies

3,696 Views
joanxie
NXP TechSupport
NXP TechSupport

each imx8mp mipi csi can support up to 4 lane, couldn't support 8 lane, but could you tell me what camera needs 8 lane?

0 Kudos
Reply

3,691 Views
MPUUser
Contributor I

Hi Joan,

I understand each MIPI can support up to 4 lanes.

Can I combine both MIPI 4 lanes to handle a single image sensor that requires 2 x 4 lanes MIPI CSI interface? One example is OMNIVISION’s OV13870. Can iMX8M Plus support this OMNIVISION image sensor? Can the iMX8M Plus merge data from both the MIPI interface to become a single image? Or it will always treat both MIPI interface as 2 separate images?

Usually image sensors with higher number of pixels (> 10MPix) will require more than 4 lanes due to the speed limitation of each lane.

0 Kudos
Reply

3,666 Views
joanxie
NXP TechSupport
NXP TechSupport

Can iMX8M Plus support this OMNIVISION image sensor?

>yes, current bsp supports ov2775 and ov5640 as default

 

Usually image sensors with higher number of pixels (> 10MPix) will require more than 4 lanes due to the speed limitation of each lane.

>imx8mp mipi csi can support 1.5Gx4=6Gbps, if your sensor is 10M@30, this is 10x30x16=4.8G<6G, and you can current ISP can support up to 12M camera, so I don't think you need use dual mipi csi to one camera

joanxie_1-1701915576036.png

 

0 Kudos
Reply

3,628 Views
joanxie
NXP TechSupport
NXP TechSupport

imx8mp doesn't support vc

0 Kudos
Reply

3,654 Views
MPUUser
Contributor I

Hi Joan,

What about OV13870. Can it be supported?

There are sensors with much higher resolution (eg 20MP) and they need 2 x 4 MIPI lanes per sensor.

Can iMX8M Plus support such sensors?

 

0 Kudos
Reply

3,643 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately imx8mp couldn't support this

0 Kudos
Reply