iMX8M Mini Use PI6CFGL201BZDIEX as PCIe REF_CLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M Mini Use PI6CFGL201BZDIEX as PCIe REF_CLK

ソリューションへジャンプ
3,592件の閲覧回数
Anonymous
適用対象外

Hi,

Following reference design, we are making custom board with iMX8M Mini but replace the default PCIe clock generator (9FGV0241AKLF) with PI6CFGL201BZDIEX.

Also, a related post https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056 indicates that PI6CFGL201BZDIEX can be used.

However, when it is replaced with PI6CFGL201BZDIEX, the driver (imx6q-pcie) will panic after reporting "PLL lock timeout". Then, kernel gets stuck and just hangs.

[ 2.677860] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.734722] imx6q-pcie 33800000.pcie: PCIe PLL lock timeout

 

Is there any driver change needed for the driver (drivers/pci/controller/dwc/pci-imx6.c )? Or, we need to change the DTS because of the replacement?

 

Thanks,

Weichen

ラベル(3)
0 件の賞賛
返信
1 解決策
3,520件の閲覧回数
Anonymous
適用対象外

Hi weidong_sun,

We tried to put the PCI module to M.2 and it worked. Like you mentioned, it seems that M.2 side of channel is working but the CPU-side doesn't. We are still investigating why it acts like this.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,539件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

these 2 clock generators are pin to pin compatible, but PIN7 and PIN5 are different definitions.

weidong_sun_0-1623726174619.png

--The clock generator can output 2-channel 100MHz clocks, one channel is for CPU side, the other is for M.2 connector.

--The clock generator doesn't need linux driver, default configuration is OK.

So now you can measure whether 100MHz clock OUPUT or not.

According to your description, obviously, CPU side doesn't get the clock input or bad clock waveform.

 

Have a nice day!

B.R,

weidong

0 件の賞賛
返信
3,521件の閲覧回数
Anonymous
適用対象外

Hi weidong_sun,

We tried to put the PCI module to M.2 and it worked. Like you mentioned, it seems that M.2 side of channel is working but the CPU-side doesn't. We are still investigating why it acts like this.

0 件の賞賛
返信