iMX8M Mini Power Sequencing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Mini Power Sequencing

1,640 Views
omar_wolfe-huss
Contributor III

Hi, 

In the data sheet for the iMX8M Mini this table is given for the power up sequence:

pastedImage_1.png

Does this mean that if all the power rails are brought up simultaneously (as the minimum time for all rails to rail delays is 0ms) and then RTC_RESET_B is released some time later full and proper operation can be expected?

Likewise if all the rails are shutdown simultaneously will there be any adverse effects?

Many thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,558 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Note, timings T1, T2, T3 are based on NVCC_SNVS_1P8 start moment,
but T4 - T13 are based on PMIC_ON_REQ, because t1 is uncertain period.

In both groups all voltages can start their rising simultaneously in the groups.

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply