iMX8M Mini GPU Profiling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M Mini GPU Profiling

3,415件の閲覧回数
banhu
Contributor I

Hello, Linux 5.4.70_2.3.0 BSP is installed IMX8M Mini.  galcore.gpuProfiler=1 is set in u-boot and as well as export VIV_PROFILE=1 in Linux environment. With glmark2-es2-wayland, I can find the vpd files. 

~# ls -lh *.vpd
-rw-r--r-- 1 root root 128 Jul  1 09:23 vprofiler_838_1.vpd
-rw-r--r-- 1 root root 19M Jul  1 09:23 vprofiler_838_2.vpd

 However the GPU utilization in VPD Analyzer is always 0% when vpd file is loaded. That is obviously not true as glmark2-es2-wayland does use GPU for rendering. The same test on iMX8M Plus shows GPU load varying from 10% to 70%. Doesn't the iMX8M Mini's GPU GC7000NanoUltra support such profiling? Thanks!

imx8mm.png

 

0 件の賞賛
返信
2 返答(返信)

3,404件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello banhu,

 

Please take a look that If you put in uboot galcore.powerManagement=0, Sometime give you some data on vpd, however this feature is not available on GC7000Nano, It suppose to be fully supported in next release of the gpu driver, you can try the 5.10.35 BSP.

Regards

0 件の賞賛
返信

3,395件の閲覧回数
banhu
Contributor I

Hi @Bio_TICFSL , thanks for replying. I will try 5.10.35 BSP later. galcore.powerManagement=0 in -uboot doesn't generate GPU utilization data. 

0 件の賞賛
返信