iMX8M Mini DDR4 x1 Calibration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8M Mini DDR4 x1 Calibration

2,822 次查看
chao
Contributor II

Hi,

We are trying to bring up our customer board which based on iMX8M Mini. The main components on the customer board are shown below:

CPU:MIMX8MM3DVTLZAA; 

DDR:MT40A512M16LY:075E(Micron), x1, 16-bits, @1333MH;

PMIC:BD71847;

 

Next,we changed some parameters in "MX8M_Mini_DDR4_RPA_v15", 

捕获.PNG

also, some other parameters in sheets have changed too, they are listed as following:

1. D43 in sheet "DDR stress test file" replaced by "0x14d032", since clock cycle freq is 1333MHz; 

2.We use I2C2 to communicate with PMIC, and configure I2C port IO pads;

 

After we downloaded the .ds file and calibrated the DDR, it loged the following message,

============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1333Mhz...
[Process] End of initialization
PMU: Error: Dbyte 0 couldn't find the rising edge of DQS during RxEn Training
PMU: ***** Assertion Error - terminating *****
[Result] FAILED

 

We referenced the post with the theme "DDR_PHY programming issue on IMX8M board" (https://community.nxp.com/t5/i-MX-Processors/DDR-PHY-programming-issue-on-IMX8M-board/m-p/970078), 

 

Unfortunately, it returned the same info  "PMU: Error: Dbyte 0 couldn't find the rising edge of DQS during RxEn Training".

So, what is the root cause of the issue?  How to fix it?

 

标签 (1)
0 项奖励
回复
2 回复数

2,109 次查看
_angelo_
Contributor III

i also have the same issue, would be nice to know if it was due to hw issues .

0 项奖励
回复

2,407 次查看
siaug18
Contributor I

Hi Did you ever fix this ? I have the same issue

 

0 项奖励
回复