Hi Igor,
thank you for the fast response.
We are able to measure some signals on the X_MIPI_DSI1_D0_P, but not on any other dataline or even the clock.
Is this normal?
I've also debuged the panel-driver to get some more information.
It is running normal, until i get the response -16 from ret = mipi_dsi_dcs_set_tear_scanline(dsi, 0x380).
from bootlog:
[ 15.531999] imx_sec_dsim_drv 32e60000.mipi_dsi: wait payload tx done time out
[ 15.543410] panel-raydium-rm67191 32e60000.mipi_dsi.0: [drm:rm67191_enable] *ERROR* Failed to set tear scanline (-16)
[ 15.554070] imx_sec_dsim_drv 32e60000.mipi_dsi: panel enable failed: -16
I've searched the sourcecode, but i can not find the meaning of it.
Maybe you can help me there.
Best Regards,
Admir