iMX8 documentation update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 documentation update

1,626 Views
NeilShipp-MSFT
Contributor II

When will the iMX8M Reference manual (IMX8MDQLQRM) be updated to fix all the errors in it?  The external signals tables are entirely missing from every section: Chapters 4.13.2, 6.5.2, 7.2.2, 8.3.2, 9.5.2, 10.1.2, 10.2.2, 10.3.2, 11.4.3, 12.2.2, 13.2.2, 13.7.2,  etc. etc.

Some sections of the document mention 3 uSDHC controllers, say table 6-17 in section 6.1.5.2.4, while Tables 2-5, 5-1, and 5-2 only list uSDHC1 and uSDHC2.  Does the iMX8m have two or three uSDHC controllers?

I'm sure there are plenty of other errors I've yet to notice.

0 Kudos
Reply
1 Reply

1,352 Views
art
NXP Employee
NXP Employee

The next release of the i.MX8M processor documentation is scheduled to the Q3 2018. Now we're collecting all bug reports to fix them in the next documentation release.

The i.MX8M series processors have only 2 uSDHC modules.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply