iMX8 - SCU ROM Passover information reading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 - SCU ROM Passover information reading

2,759件の閲覧回数
Ansari
Contributor IV

Hi Team,

Currently we are using i.MX8DX6-B0 silicon based custom platform along with 4.14.78 GA BSP release.

We have referred the document https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf

From the above mentioned document "5.12.2 SCU ROM Passover" section explains about SCU ROM passover information(added in attachment). We would like to read the SCU ROM passover information to get the values of the "Image set booted from" field.

We understood that this field will give the information about 1st/2nd Image container set which is booted from.

Could you help us on this.

Thanks and Regards,

Ansari

0 件の賞賛
返信
2 返答(返信)

2,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ansari

document was provided via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,392件の閲覧回数
peter82
Contributor I

Could you please provide the document for me as well?

0 件の賞賛
返信