iMX7D: Simulating LPDDR3 with Hyperlynx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7D: Simulating LPDDR3 with Hyperlynx

2,580 Views
noeliascotti80
Contributor I

I am doing pre-layout simulation in order to start the PCB design, but I have doubts.
1. I don't find the recommended trace impedance for the LPDDR3 memory in the hardware development guide. The recommended value is only for DDR3 memory, not for LPDDR3. Micron recommends 60 ohm for single ended and 120 ohm for differential pairs. Which value is the correct impedance for LPDDR3 memory?
2. The iMX7 IBIS model doesn't have the Diff pin section, it is a problem for the DDR simulation. Do you have a complete model? We added the diff pin section manually but I don't know if it is fine. I don't know the vdiff value.

[Diff Pin] inv_pin vdiff tdelay_typ tdelay_min tdelay_max
AF25 AE25 0.000V 0.000s NA NA
AG23 AG24 0.000V 0.000s NA NA
AC20 AB20 0.000V 0.000s NA NA
AD27 AC27 0.000V 0.000s NA NA
Y24 Y23 0.000V 0.000s NA NA

Thanks!

Labels (1)
0 Kudos
Reply
3 Replies

2,291 Views
noeliascotti80
Contributor I

My case has never been answered.

- In the recent Hardware Guide there is no special recommendation for LPDDR3 memory. I think it is not the same routing DDR3 or LPDDR3.

- IBIS model does support differential signals. I don't understand why the iMX7 model does not have diff pin section. iMX6 model has diff pin section.

Thanks!

0 Kudos
Reply

2,291 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please look at Table 19 (DDR trace routing guidelines) of Hardware

Development Guide for i.MX7Dual and 7Solo Applications Processors,

Rev. 1, 07/2017.

Regards,

Yuri.

0 Kudos
Reply

2,291 Views
igorpadykov
NXP Employee
NXP Employee

Hi Noelia

seems this was already answered on ticket:

-recommended to follow memory  rules, published in the recent Hardware Guide

 http://www.nxp.com/assets/documents/data/en/user-guides/IMX7DSHDG.pdf

- IBIS model does not support differential signals. One of possible approach is
to treat with differential signals using single-ended data.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply