iMX7D : External clock input timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7D : External clock input timing

ソリューションへジャンプ
1,648件の閲覧回数
koichisakagami
Contributor II

Dear community,
We have been developing our product with iMX7D.

I have a question about  iMX7D inputting clock timing.

In Data sheet IMX7DCEC Rev. 2 , 4.2.1 Power-up sequence,
it is described that the power-up sequence about POR_B and VDD_xxx signal are defined.
But the 24MHz and 32kHz external clock signal sequence are not defined.

[Question]
In the case of using an external oscillator instead of crystal,
Could you teach me the timing to begin feeding the clock signal to iMX7 ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,536件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

clock can be provided simultaneously with power for oscillator circuits:

VDD_SNVS for 32kHz and VDD_XTAL_1P8 for 24MHz.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,537件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

clock can be provided simultaneously with power for oscillator circuits:

VDD_SNVS for 32kHz and VDD_XTAL_1P8 for 24MHz.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信