iMX7 memory region control in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 memory region control in u-boot

1,542 Views
timholland
Contributor I

I want to set memory region restrictions in u-boot and I can't find much information.

I can see that RDC functions have been added to allow control of peripheral devices and asign them to domains, but memory regions don't seem to be implemented.

Has anybody done this?

Labels (1)
0 Kudos
Reply
1 Reply

1,366 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tim

I am afraid it is not supported, in general one can post it on

https://lists.denx.de/listinfo/u-boot 

also may be useful to check attached Porting Guide Chapter 1 Porting U-Boot

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply