iMX7 ethernet problem on Linux 4.14, NETDEV WATCHDOG: eth0 (fec): transmit queue 1 timed out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 ethernet problem on Linux 4.14, NETDEV WATCHDOG: eth0 (fec): transmit queue 1 timed out

2,749 Views
alpha_one_x86
Contributor I

Hi,

With direct + forward trafic with iperf3 on Linux 4.14 I have NETDEV WATCHDOG: eth0 (fec): transmit queue 1 timed out.

Hardware: IOT-GATE-iMX7, compulab,NXP i.MX 7Dual ARM Cortex-A7

See the attached file. How fix it?

Cheers.

0 Kudos
Reply
3 Replies

2,500 Views
alpha_one_x86
Contributor I

Hi,

Thanks for your reply.

I need a particular features of 4.14, then I need 4.14+ only.

Compulab don't have time to fix this issue.

Cheers,

0 Kudos
Reply

2,500 Views
igorpadykov
NXP Employee
NXP Employee

please read support policy on

FSL Community BSP Release Notes 2.2 documentation 

---------------------------------------------------------------------------------------------------

Machine Maintainershttp://freescale.github.io/doc/release-notes/2.2/#machine-maintainers

every new board must have someone assigned as maintainer. This ensures, in long term, all boards with a maintainer assigned. Current orphan boards are not going to be removed unless it causes maintenance problem and the fix is not straightforward.

The maintainer duties:
  • The one with casting vote when a deadlock is faced.
  • Responsible to keep that machine working (that means, booting and with some stability) Keep kernel, u-boot updated/tested/working.
  • Keep release notes updated
  • Keep test cycle updated
  • Keep the most usual images building and booting

When a build error is detected, the maintainer will “fix” it.

----------------------------------------------------------------------------------------------------

alternatively you can apply to

NXP Professional Services|NXP 

Best regards
igor

0 Kudos
Reply

2,500 Views
igorpadykov
NXP Employee
NXP Employee

Hi Herman

Linux 4.14 is not supported linux version by nxp, please try for example L4.1.15

described on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Issues with Linux 4.14 can be posted on compulab forum or meta-fsl-arm mailing list,

so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply