iMX7 dual - Temperature issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7 dual - Temperature issue

2,416件の閲覧回数
yuvarajviswanat
Contributor I

Hi,

We are facing a temperature issue in iMX7 dual processor (commercial).The part number is "MCIMX7D7DVM10SC". The processors undergoes thermal shutdown at 60'C (ambient) with just a single Ethernet interface operating @ 100Mbps. Later I repeated the experiment with iMX7-Sabre SD and Nitrogen boards and got the results mentioned below.

Table.1 Results of Experiments

BoardSabre SDOur ProductNitrogen
Interface runningEthernet x1 @100MbpsEthernet x1 @100MbpsEthernet x1 @100Mbps
Ambient Temperature67.3'C63.5'C82'C
Die temperature @Thermal shutdown90'C90'C105'C(Industrial processor)
Temperature on processor package top @Thermal shutdown83.3'C83.7'C97.3'C

The total power consumed by our product is 1W (Max). As per the datasheet specification the Junction to Package temperature is 0.2'C/W (shown in below table).

pastedImage_9.pngThe expected temperature difference between the Die temperature and the Temperature on the processor package must be 0.2'C (for our case). But from  table.1 it is clear that the difference is too large.

Moreover the CPU load is about 30-35%.

Looking forward for suggestions.

Thanks for your interest,

Yuvaraj

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,101件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuvaraj

suggestions for controlling chip temperature are provided in

AN4579 i.MX6 Series Thermal Management Guidelines (also valid for i.MX7)

https://www.nxp.com/docs/en/application-note/AN4579.pdf 

As processor operates at 60'C ambient temperature, it temperature will be

higher by "Junction to Ambient" factor using Table.1 (upper two rows) .

In Linux Thermal driver handles processor temperature, it is described in

Chapter 25 Thermal Driver attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信