Latency Issue - I.MX6Q/D boundary devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latency Issue - I.MX6Q/D boundary devices

1,171 Views
rajvikamdar
Contributor III

I am having aroud 400ms latency issue with I.MX6 device.

Using Android kitkat, with miracast, H264 Open MAX decoder. Kernel version 3.10.

Have already tried the following methods:

1. Have checked by enabling VPU_352M parameter in kernel, no difference in latency.

2. Modified and checked wifi parameters and enabled 5Ghz further.

Needed help to reduce the latency on firmware Linux encoder decoder side or Android Framework Side.

0 Kudos
Reply
4 Replies

792 Views
rajvikamdar
Contributor III

Hi Igor

Thank you for the post. It seems that he is having the same issue as me. There is not much response on the same.

Requesting if you could help more with the same.

Regards

Rajvi

0 Kudos
Reply

792 Views
rajvikamdar
Contributor III

Thank you for your reply. But following both the posts does not solve my issue. I am still getting latency 300-400ms.

I read a few posts related to this, and found that latency depends on

num_reorder_frames, max_dec_frame_buffering,

num_ref_frames, MaxDpbSize. Can you help me debug further into this. And help in modifying the parameter values.

Nitrogen 6X -- large streaming delay.

We won't be able to have commercial production if this does not get solved. Requesting if help be provided on urgent basis.

0 Kudos
Reply

792 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

792 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rajvi

for vpu latencies one can look at

Video delay problem in Android 

in general miracast is supported with Professional Services

Miracast for Linux|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply