iMX6ull ethernet problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ull ethernet problem

Jump to solution
5,495 Views
guochgz
Contributor III

hi, all:

      the phy chip for our board is KSZ8081RNBIA1913A3M, now after kernel is loaded, the network is not working. 

pastedImage_2.png

   

     pastedImage_4.png

pastedImage_5.png

pastedImage_6.png

      the host (192.168.8.5) is my pc's address.

Labels (2)
1 Solution
5,143 Views
guochgz
Contributor III

Hi, igor.

      In my boards, We have checked that, our MDIO/MDC pins to change to ENET2_RX_DATA0/1, and RST pin changes to CSI_HSYNC(F3). INT pin keep the same, linked to the SNVS_TAMPER5.

      pastedImage_1.png

pastedImage_2.png

    

   after above changes, we got log like this:

   libphy: Neil.zhang added here, addr = 2, phy_id = ffffffff

   pastedImage_3.png

it seems that the KSZ8081 chip is not working or mdio dts configure err? 

edit2:

      add some info that in uboot env.

      


Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
Net: FEC0
Error: FEC0 address not set.

Normal Boot
Hit any key to stop autoboot: 0
=> mii info
PHY 0x02: OUI = 0x0885, Model = 0x16, Rev = 0x01, 100baseT, FDX
=> mdio read 0x1
Reading from bus FEC0
PHY at address 0:
1 - 0xffff
=> mdio read 0x2
Reading from bus FEC0
PHY at address 0:
2 - 0xffff
=> mdio read 0x3
Reading from bus FEC0
PHY at address 0:
3 - 0xffff
=> mdio
mdio - MDIO utility commands

Usage:
mdio list - List MDIO buses
mdio read <phydev> [<devad>.]<reg> - read PHY's register at <devad>.<reg>
mdio write <phydev> [<devad>.]<reg> <data> - write PHY's register at <devad>.<reg>
mdio rx <phydev> [<devad>.]<reg> - read PHY's extended register at <devad>.<reg>
mdio wx <phydev> [<devad>.]<reg> <data> - write PHY's extended register at <devad>.<reg>
<phydev> may be:
<busname> <addr>
<addr>
<eth name>
<addr> <devad>, and <reg> may be ranges, e.g. 1-5.4-0x1f.

View solution in original post

0 Kudos
Reply
5 Replies
5,143 Views
igorpadykov
NXP Employee
NXP Employee

Hi 国承 张 

one can check enet clock with oscilloscope and debug it in function

setup_fec(int fec_id) paying attention to clock direction set by IOMUX_GPR1

mx6ullevk.c\mx6ullevk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,142 Views
guochgz
Contributor III

thanks igor.

our baseline is L4.1.15

on my board, I have check that ENET1_TX_CLK is 50Mhz, and ENET1_nRST is low.

and in the file uboot/include/configs/imx6ullevk.h, I have change the CONFIG_FEC_ENET_DEV from 1 to 0. because on my board, there is only one phy for ENET1.

and after set env in uboot, this is no mii info on my board.

pastedImage_1.png

pastedImage_2.png

   and when I ping the host connected my board, the uboot reset...

   pastedImage_3.png

     in kernel. I have do some follow changes:

      pastedImage_4.png

      pastedImage_5.png

      pastedImage_7.png

      pastedImage_8.png

        

      and the left led of the RJ45 port is off status.

      is there any other suggestions?  

0 Kudos
Reply
5,142 Views
igorpadykov
NXP Employee
NXP Employee

so had you checked enet clock with oscilloscope, is it present?

0 Kudos
Reply
5,144 Views
guochgz
Contributor III

Hi, igor.

      In my boards, We have checked that, our MDIO/MDC pins to change to ENET2_RX_DATA0/1, and RST pin changes to CSI_HSYNC(F3). INT pin keep the same, linked to the SNVS_TAMPER5.

      pastedImage_1.png

pastedImage_2.png

    

   after above changes, we got log like this:

   libphy: Neil.zhang added here, addr = 2, phy_id = ffffffff

   pastedImage_3.png

it seems that the KSZ8081 chip is not working or mdio dts configure err? 

edit2:

      add some info that in uboot env.

      


Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
Net: FEC0
Error: FEC0 address not set.

Normal Boot
Hit any key to stop autoboot: 0
=> mii info
PHY 0x02: OUI = 0x0885, Model = 0x16, Rev = 0x01, 100baseT, FDX
=> mdio read 0x1
Reading from bus FEC0
PHY at address 0:
1 - 0xffff
=> mdio read 0x2
Reading from bus FEC0
PHY at address 0:
2 - 0xffff
=> mdio read 0x3
Reading from bus FEC0
PHY at address 0:
3 - 0xffff
=> mdio
mdio - MDIO utility commands

Usage:
mdio list - List MDIO buses
mdio read <phydev> [<devad>.]<reg> - read PHY's register at <devad>.<reg>
mdio write <phydev> [<devad>.]<reg> <data> - write PHY's register at <devad>.<reg>
mdio rx <phydev> [<devad>.]<reg> - read PHY's extended register at <devad>.<reg>
mdio wx <phydev> [<devad>.]<reg> <data> - write PHY's extended register at <devad>.<reg>
<phydev> may be:
<busname> <addr>
<addr>
<eth name>
<addr> <devad>, and <reg> may be ranges, e.g. 1-5.4-0x1f.

0 Kudos
Reply
5,142 Views
guochgz
Contributor III

yes, I have checked. 

I have add some log in my baseline L4.1.15, found that phydev->phy_id is zero, does this means the phy chip is not work ? 

fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 66:14:2a:50:c3:1a
Neil.zhang added here, before of_mdiobus_register
libphy: Neil.zhang added here, mido_register begin...
libphy: fec_enet_mii_bus: probed
libphy: Neil.zhang added here, phy_device_register
libphy: Neil.zhang added here, phy_scan_fixups
libphy: Neil.zhang added here, phy_uid = 221560, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_id is 0, uid = 221560, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_needs_fixup ret false, phy_uid = 221560, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_uid = 221561, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_id is 0, uid = 221561, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_needs_fixup ret false, phy_uid = 221561, uid_mask = ffffffff
Neil.zhang added here, phy_device_register ret zero
mdio_bus 2188000.ethernet: registered phy ethernet-phy at address 2
libphy: Neil.zhang added here, phy_device_register
libphy: Neil.zhang added here, phy_scan_fixups
libphy: Neil.zhang added here, phy_uid = 221560, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_id is 0, uid = 221560, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_needs_fixup ret false, phy_uid = 221560, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_uid = 221561, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_id is 0, uid = 221561, uid_mask = ffffffff
libphy: Neil.zhang added here, phy_needs_fixup ret false, phy_uid = 221561, uid_mask = ffffffff
Neil.zhang added here, phy_device_register ret zero
mdio_bus 2188000.ethernet: registered phy ethernet-phy at address 1

another question ? what about you mean that check IOMUXC_GPR, I have no idea about that.

pastedImage_7.png

for full dmesg log, please refer to attachment.

edit 2st: 

pastedImage_1.png