iMX6qsabresd--TFTP&NFS problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6qsabresd--TFTP&NFS problem

3,485件の閲覧回数
zhangmeiyu
Contributor I

Hi :

I have started ubuntu14.04.1 on the board through i.MX6q SABRE Board for Smart Devices - Linux on ARM - eewiki   ,all the things needed are in the SD card.Now i want to start the linux kernel through TFTP and access the rootfs on the host via NFS.Through the first way I got the image file named zImage and the rootfs supposed it named ubuntu14.04.1. I have put them in the TFTP shared directory and NFS shared directory in the host.Then I should set the parameters on the UBOOT command line which has done as follow:

setenv ipaddr  <myipaddr>

setenv serverip <my serverip>

setenv gatewayip <my gatewayip>

setenv ehtaddr <my ethaddr>

setenv ip_dyn no 

setenv nfsroot /home/nfs

setenv image zImage

setenv loadaddr 0x12000000

ok,the problem is that,I don't know how to set the remaining parameters such as bootargs,bootcmd or more else…… 

And I want to know if the image and the rootfs I used are correct, if not ,can someone provide me a correct one?

Thanks a lot .

Mary 

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

3,060件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Please use "i.MX Linux® User's Guide" of NXP Linux BSP docs,
in particular sections  4.7 (Running Linux OS on the target),
4.7.5 (Running the Linux image from NFS), 4.4.1.1 (Downloading
an image to MMC/SD).

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,060件の閲覧回数
zhangmeiyu
Contributor I

Hi Yuri,

Thanks for replying.

I have followed the "i.MX Linux® User's Guide",in particular sections you said,but it still doesn't work .Here are my settings and the start information

Hit any key to stop autoboot:  0                                                                                                                                               

=> print                                                                                                                                                                       

baudrate=115200                                                                                                                                                                 

boot_fdt=try                                                                                                                                                                    

bootcmd=setenv mmcdev 1;setenv mmckernel 0;run mmcboot;setenv mmcdev 0;setenv mmckernel 0;run mmcboot;                                                                         

bootdelay=1                                                                                                                                                                     

bootscript=echo Running bootscript from mmc ...; source                                                                                                                         

console=ttymxc0,115200                                                                                                                                                         

emmcdev=2                                                                                                                                                                       

ethact=FEC                                                                                                                                                                      

ethaddr=00:04:9f:03:ef:78                                                                                                                                                      

ethprime=FEC                                                                                                                                                                    

fdt_addr=0x18000000                                                                                                                                                             

fdt_file=imx6q-sabresd.dtb                                                                                                                                                     

fdt_high=0xffffffff                                                                                                                                                            

image=zImage                                                                                                                                                                    

initrd_high=0xffffffff                                                                                                                                                          

ip_dyn=yes                                                                                                                                                                     

loadaddr=0x12000000                                                                                                                                                             

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};                                                                                                          

loadfdt=echo loading ${fdtdir}/${fdt_file} ...;  load mmc ${bootpart} ${fdt_addr} ${fdtdir}/${fdt_file}                                                                        

loadimage=load mmc ${bootpart} ${loadaddr} ${bootdir}/${bootfile}                                                                                                              

loadrd=load mmc ${bootpart} ${rdaddr} ${bootdir}/${rdfile}; setenv rdsize ${filesize}                                                                                           

mmcargs=setenv bootargs console=${console}${optargs} root=${mmcroot} rootfstype=${mmcrootfstype} ${cmdline}                                                                    

mmcboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};setenv bootpart ${mmcdev}:1; echo Checking for: /uEnv.txt ...;if test -e mmc ${bootpart} /;

mmcboot_old=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if tes;

mmcdev=1                                                                                                                                                                       

mmcpart=1                                                                                                                                                                      

mmcroot=/dev/mmcblk0p2 ro                                                                                                                                                       

mmcrootfstype=ext4 rootwait fixrtc                                                                                                                                              

netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp                                                             

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes;

rdaddr=0x12A00000                                                                                                                                                               

script=boot.scr                                                                                                                                                                

uname_boot=setenv bootdir /boot; setenv bootfile vmlinuz-${uname_r}; if test -e mmc ${bootpart} ${bootdir}/${bootfile}; then echo loading ${bootdir}/${bootfile} ...; run loadi;

update_emmc_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if ${get_cmd} ${update_sd_firmware_filename}; then if mmc dev ${emmcdev} i

update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmware_filename}; thi

                                                                                                                                                                                

Environment size: 5040/8188 bytes                                                                                                                                               

=> setenv serverip 192.168.1.18                                                                                                                                                

=> setenv bootfile zImage                                                                                                                                                      

=> setenv fdt_file imx6q-sabresd                                                                                                                                                

=> setenv ethaddr 00:04:9F:03:EF:78                                                                                                                                             

=> saveenv                                                                                                                                                                      

Saving Environment to MMC...                                                                                                                                                    

Writing to MMC(1)... done                                                                                                                                                       

=> dhcp                                                                                                                                                                        

BOOTP broadcast 1                                                                                                                                                               

BOOTP broadcast 2                                                                                                                                                               

*** Unhandled DHCP Option in OFFER/ACK: 52                                                                                                                                     

*** Unhandled DHCP Option in OFFER/ACK: 52                                                                                                                                     

DHCP client bound to address 192.168.1.16 (1002 ms)                                                                                                                             

Using FEC device                                                                                                                                                               

TFTP from server 192.168.1.18; our IP address is 192.168.1.16                                                                                                                  

Filename ''.                                                                                                                                                                   

Load address: 0x12000000                                                                                                                                                        

Loading: *                                                                                                                                                                     

TFTP error: 'File not found' (1)                                                                                                                                                

Not retrying...                                                                                                                                                                 

=> setenv ipaddr 192.168.1.17                                                                                                                                                  

=> save                                                                                                                                                                         

Saving Environment to MMC...                                                                                                                                                    

Writing to MMC(1)... done                                                                                                                                                      

=> mmc dev                                                                                                                                                                      

MMC: no card present                                                                                                                                                            

=> tftpboot ${fdt_addr} ${fdt_file}                                                                                                                                            

Using FEC device                                                                                                                                                               

TFTP from server 192.168.1.18; our IP address is 192.168.1.17                                                                                                                   

Filename 'imx6q-sabresd'.                                                                                                                                                       

Load address: 0x18000000                                                                                                                                                       

Loading: *                                                                                                                                                                      

TFTP error: 'File not found' (1)                                                                                                                                                

Not retrying...                                                                                                                                                                

=> mmc write ${fdt_addr} 0x5000 0x800                                                                                                                                           

MMC: no card present                                                                                                                                                            

=> setenv consoleinfo 'console=ttymxc0,115200'                                                                                                                                 

=> setenv loadaddr 0x12000000                                                                                                                                                   

=> setenv fdt_addr 0x18000000                                                                                                                                                  

Unknown command 'setenv' - try 'help'                                                                                                                                         

=> setenv fdt_addr 0x18000000                                                                                                                                                  

=> setenv fdt_file 'imx6q-sabresd.dtb'                                                                                                                                          

=> setenv rootfsinfo 'root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp'                                                                                              

=> setenv rootfsinfo 'root=/dev/nfs ip=dhcp weim-nor nfsroot=${serverip}:${nfsroot},v3,tcp'                                                                                    

=> setenv rootfsinfo 'ubi.mtd=3 root=ubi0:rootfs rootfstype=ubifs rootwait rw mtdparts=gpmi-nand:16m(boot),16m(kernel),16m(dtb),-(rootfs)'                                     

=> setenv rootfsinfo 'root=/dev/mmcblk0p2 rootwait rw'                                                                                                                          

=> setenv bootargsset 'setenv bootargs ${consoleinfo} ${rootfsinfo} ${displayinfo} ${special}'                                                                                 

=> setenv bootcmd 'run bootargsset; {settings for device}; bootz ${loadaddr} - ${fdt_addr}'                                                                                    

=> setenv rootfsinfo 'setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:/home/nfs,v3,tcp'                                                                   

=> setenv bootcmd_net 'run rootfsinfo; dhcp ${image}; dhcp ${fdt_addr} ${fdt_file}; bootz ${loadaddr} - ${fdt_addr}'                                                           

=> setenv bootcmd 'run bootcmd_net'                                                                                                                                            

=> saveenv                                                                                                                                                                      

Saving Environment to MMC...                                                                                                                                                   

Writing to MMC(1)... done                                                                                                                                                      

=>

 

restart

start information

 

U-Boot 2014.10-dirty (Mar 15 2017 - 20:03:15)                                                                                                                                   

                                                                                                                                                                                

CPU:   Freescale i.MX6D rev1.2 at 792 MHz                                                                                                                                      

Reset cause: POR                                                                                                                                                                

Board: MX6-SabreSD                                                                                                                                                              

I2C:   ready                                                                                                                                                                   

DRAM:  1 GiB                                                                                                                                                                    

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2                                                                                                                                    

MMC: no card present                                                                                                                                                           

MMC init failed                                                                                                                                                                 

Using default environment                                                                                                                                                       

                                                                                                                                                                               

No panel detected: default to Hannstar-XGA                                                                                                                                     

Display: Hannstar-XGA (1024x768)                                                                                                                                               

In:    serial                                                                                                                                                                   

Out:   serial                                                                                                                                                                   

Err:   serial                                                                                                                                                                  

PMIC:  PFUZE100 ID=0x10                                                                                                                                                         

Net:   FEC [PRIME]                                                                                                                                                              

Hit any key to stop autoboot:  0                                                                                                                                               

MMC: no card present                                                                                                                                                            

MMC: no card present                                                                                                                                                            

MMC: no card present                                                                                                                                                           

MMC: no card present                                                                                                                                                            

=>

so,when save the environment variable,it  shows 

=> saveenv                                                                                                                                                                      

Saving Environment to MMC...                                                                                                                                                   

Writing to MMC(1)... done  

but it shows 

MMC: no card present    

What should I do with it?

Regards,

Mary

0 件の賞賛
返信

3,060件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 > TFTP error: 'File not found' (1)      

  Looks like FTP server is not set properly or it does not contain the needed files.

What are FTP server settings ?

Regards,

Yuri.

0 件の賞賛
返信

3,060件の閲覧回数
zhangmeiyu
Contributor I

hi,

My TFTP server is  built on my PC's virtual machine.

zmy@zmy-virtual-machine:~$ sudo /etc/init.d/xinetd restart
[sudo] password for zmy:
* Stopping internet superserver xinetd [ OK ]
* Starting internet superserver xinetd [ OK ]
zmy@zmy-virtual-machine:~$ sudo netstat -a|grep tftp
udp 0 0 *:tftp *:*


 then I test it again ,the result is as follows,it also success


root@zmy-virtual-machine:~# cd /var
root@zmy-virtual-machine:/var# tftp localhost
tftp> get test
tftp> q
root@zmy-virtual-machine:/var# cat test
success le hahahahaha
root@zmy-virtual-machine:/var#

My TFTP share directory has the file as follows:

pastedImage_1.png

Regards,

Mary

0 件の賞賛
返信

3,060件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the following may be helpful :

https://community.nxp.com/docs/DOC-103717 

Regards,

Yuri.

0 件の賞賛
返信