iMX6ULL cpu frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL cpu frequency

3,668 Views
aermakov
Contributor II

I am using cpu iMX6ULL, and I need to set CPU and system bus frequency manually.

Linux devicetree have several presets for CPU and soc frequency. Can I add there my custom value (It will be multiply 24)?

And how do I know the voltage for this frequency?

Labels (1)
0 Kudos
Reply
5 Replies

3,478 Views
Yuri
NXP Employee
NXP Employee

Hello,

Theoretically it is possible to add new custom working setpoints, but hardly it may

be recommended, since - because of system complexity - it will require much efforts

to debug and test new setpoints for all conditions.

Regards,

Yuri.

0 Kudos
Reply

3,478 Views
aermakov
Contributor II

What are the setpoints? Is it CPU frequency and voltage, and SOC frequency and voltage? Are the SOC and CPU frequencies related, or are they set separately from each other?

We have the ability to test setpoints in different conditions.

0 Kudos
Reply

3,478 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Use sections  2.5.3 [CPU Frequency Scaling (CPUFREQ)] and  2.5.4 (Dynamic Bus

Frequency) of the i.MX Linux Reference Manual for more details.

 

https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga

imx6ul.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Regards,

Yuri.

0 Kudos
Reply

3,478 Views
aermakov
Contributor II

Latest linux kernel version with busfreq driver I found is 4.9 at the git://git.freescale.com/imx/linux-imx.git repository. Is there newer kernel version with busfreq driver?

0 Kudos
Reply

3,478 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Look at Table 2-15 (BusFrequency Driver Files) in "i.MX_Reference_Manual.pdf".

https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga

Regards,

Yuri.

0 Kudos
Reply