iMX6ULL boot form eMMC setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6ULL boot form eMMC setting

4,248 次查看
paultran
Contributor I

hi, i make mainboard with imx6ull and boot defaulf from eMMC. 

but it can not work well. 

attached is booting setup resistor via HW and circuit of eMMC design, i follow NXP ref design. 

anybody have any suggest for bring up or debug. 

thanks

标签 (2)
0 项奖励
回复
1 回复

4,052 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Paul

one can check with jtag boot configuration in SRC_SBMR1,2,

if it was correctly sampled. Also useful to check 24MHZ, 32.768kHz clocks

and prolong POR up to 1 sec. Then follow debug procedure described on

https://community.nxp.com/thread/307723 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复