PCMCIA for M9328MX21ADSE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCMCIA for M9328MX21ADSE

ソリューションへジャンプ
1,960件の閲覧回数
rayangli
Contributor I

Dears !

     the datasheet doesn't provide more information about PCMCIA, only provide the description about signals.

     So, could the i.MX21(M9328MX21ADSE) support the usage of  I/O devices.

    thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
1,854件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rayang

if necessary, you can obtain i.MX21 ADS PCMCIA daughter card schematic creating service request.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,855件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rayang

if necessary, you can obtain i.MX21 ADS PCMCIA daughter card schematic creating service request.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,854件の閲覧回数
rayangli
Contributor I
I found it !
“PCMCIA/CF host controller interface compliant with the PCMCIA standard release 2.1 (for I/O Cards) and fully compliant with the Compact Flash Specification V1.4” on i.MX21 Applications Processor Reference Manual.
thanks~
0 件の賞賛
返信