iMX6ULL DDR3L part number related query?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL DDR3L part number related query?

1,810 Views
ramesh6663
Contributor III

We are planing to use `Kingston DDR3L part D2516ECMDXGJDI-U. Which has 933Mhz operating frequency range and 1866 data rate speed.

If iMx6ull maximum frequency mentioned 400Mhz and we are going to use 933Mhz DDR3l chip is it ok?

Thanks & Regards,

Rameshkumar 

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,616 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rameshkumar 

yes this is ok, one can select max. available speed in

ddr script aid, for example sellect 1600 grade for 1866 grade design.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,616 Views
ramesh6663
Contributor III

Dear Igor,

 Thanks for your quick reply. So while doing DDR3 calibration I can enter the speed grade of the device(.xls) which used , Like said 933Mhz and i can run the script, It will provide the result going to incorporated in Uboot. Am i right?

Thanks & regards,

Rameskumar

0 Kudos
Reply

1,616 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rameshkumar 

right

Best regards
igor

0 Kudos
Reply

1,616 Views
ramesh6663
Contributor III

Dear Igor,

 

 Thanks for your quick reply.

 

Thanks & regards,

Rameskumar

0 Kudos
Reply