iMX6ULL DDR IO pad reassignment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6ULL DDR IO pad reassignment

ソリューションへジャンプ
2,193件の閲覧回数
mobileoverlord
Contributor II

According to the Hardware design guide Section 3.5.1 discusses data line swapping for the DDR routing configuration. It has the following note:

If the byte lane swapping was done, the target DDR IC register read value must be transposed according to the data line swapping.

The Hardware reference IO pin max configuration section 4.1.1 describes the MMDC DATA* pins are muxed to their corresponding pads with No Mixing (ALT0). I am under the impression that I need to remap this pin to pad mux to reflect the four data line swaps that were made in the custom layout I am working with. In my layout D1 & D4 are swapped and D2 & D7 are swapped. Please advise what changes need to be reflected in the registers. Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,185件の閲覧回数
mobileoverlord
Contributor II

sorry, I think I misunderstood the requirements. I believe I only need to ensure the pad configuration is set for all DDR data pins in use. The bit swapping will “just work”

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,162件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mobileoverlord 

I hope you are doing well.

I think your issue is resolved. Can i mark this ticket to close state?

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信
2,158件の閲覧回数
mobileoverlord
Contributor II

Should be OK thanks

0 件の賞賛
返信
2,186件の閲覧回数
mobileoverlord
Contributor II

sorry, I think I misunderstood the requirements. I believe I only need to ensure the pad configuration is set for all DDR data pins in use. The bit swapping will “just work”

0 件の賞賛
返信