iMX6UL - eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL - eMMC

3,993 Views
riteshpatel
Contributor II

Hi,

 

I am using iMX6UL in my design with JEDEC/MMC version 4.51 compliant eMMC MTFC4GACAAAM-1M WT. The eMMC part i am planning to use is not recommended for new design.

So I want to move to new part which is MMC version 5.0 compliant eMMC MTFC4GACAJCN-1M WT.

As per datasheet iMX6UL supports MMC version 4.4/4.5.

Can i use ver 5.0 compliant eMMC MTFC4GACAJCN-1M WT with iMX6UL processor.?

 

Seeking for help.

Thank you.

Original Attachment has been moved to: Micron_eMMC.zip

Labels (1)
0 Kudos
Reply
2 Replies

2,174 Views
linda_zhang
Contributor IV

5.0 eMMC can be used, we are using 5.0 MTFC4GACAJCN-4M IT part on our i.MX 6ul/6ull board MYD-Y6ULX 

0 Kudos
Reply

2,174 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ritesh Patel,

You should be able to use the eMMC 5.0 but none of the 5.0 specific features will be available. You would be using it as a eMMC 4.4/4.5. For this you would need to change the value of card->ext_csd.rev from 6 to 7. You may find more information on the thread below, it's not i.MX6UL specific but the logic would be the same.

i.mx6 with eMMC 5.0 SDR or DDR interface?

Regards,

0 Kudos
Reply