iMX6UL Video with OSD Overlay

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6UL Video with OSD Overlay

1,791 次查看
keithgill
Contributor I

I am using an iMX6UL with Gstreamer and want to add and OSD (bitmap) on top of live video, 

My current pipeline is gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! videobox border-alpha=0.5 fill=1 top=-20 bottom=-20 left=-20 right=-20 ! imxvideoconvert_pxp rotation=horizontal-flip ! imxv4l2sink

Is there any example how to add a bitmap overlay ?

0 项奖励
回复
1 回复

1,472 次查看
art
NXP Employee
NXP Employee

The i.MX6UL processor does not have the graphics acceleration in hardware, so, no overlaying is supported on it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复