iMX6UL Video with OSD Overlay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL Video with OSD Overlay

1,793件の閲覧回数
keithgill
Contributor I

I am using an iMX6UL with Gstreamer and want to add and OSD (bitmap) on top of live video, 

My current pipeline is gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! videobox border-alpha=0.5 fill=1 top=-20 bottom=-20 left=-20 right=-20 ! imxvideoconvert_pxp rotation=horizontal-flip ! imxv4l2sink

Is there any example how to add a bitmap overlay ?

0 件の賞賛
返信
1 返信

1,474件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6UL processor does not have the graphics acceleration in hardware, so, no overlaying is supported on it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信