iMX6UL USB over current functionality

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL USB over current functionality

2,144 Views
hansjpetersen
Contributor I

Using the iMX6UL as a USB host controller, with an external power switch with over current status.

If I wire the OC status to a iMX6UL OC pin (as described in table 54-1 of the iMX6UL Reference Manual). Will there be any HW dependencies when a OC situation occurs:

1: Activating the OC input, will the USB data transfer be interrupted?

2: Will the OC input by any means directly control the PWR output?

I am thinking of any HW links between functions of the USB block.

A lot of reference designs are using any other GPIO pin for OC status, which I assume requires the USB driver to be adapted to that. But as the Reference Manual lists a number of dedicated pins for OC status, I'm wondering if the chip itself has any HW functionality for handling OC situations.

Labels (1)
1 Reply

1,911 Views
RossMcLuckie
NXP Employee
NXP Employee