Hi Jim
>For example, if the SD card has been already inserted, how I know iMX6UL detect this device well?
linux detects device in probe function of wifi module, as example one can refer to BCM4339 driver sources
described in Linux Manual Chapter 46 Wi-Fi BCM4339 Driver, included in linux documentation package
https://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=13376994810717061...
>can I detect Wifi module via SDIO before Wifi driver porting?
I am afraid no. In general usdhc interface can be tested with unit tests (../test/mxc_mmc_test)
imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------